Phase Offset (Trace Format)
Phase Offset specifies the phase offset for the and options.
When the selected is , offsets the phase trace by the amount of phase shift specified in the text box. For example, a phase offset of 90 degrees offsets the phase trace by +90 degrees, such that a phase value of 0 degrees will be shown on the trace as +90 degrees .
This parameter is only available for the selections: and .
See Also